public static class ObjectBuilder.BuilderVersion extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE
linked feature can directly select the product interface item
|
static int |
_ORIGINAL
linked feature cannot select the product interface item
|
static int |
_THREE
Enables product interface types but used along with the 'Enable Product Interface Type' customer default
|
static int |
_TWO
product interface builder supports composite curve, composite face and body collector options
|
static ObjectBuilder.BuilderVersion |
ONE
linked feature can directly select the product interface item
|
static ObjectBuilder.BuilderVersion |
ORIGINAL
linked feature cannot select the product interface item
|
static ObjectBuilder.BuilderVersion |
THREE
Enables product interface types but used along with the 'Enable Product Interface Type' customer default
|
static ObjectBuilder.BuilderVersion |
TWO
product interface builder supports composite curve, composite face and body collector options
|
Modifier and Type | Method and Description |
---|---|
static ObjectBuilder.BuilderVersion |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ObjectBuilder.BuilderVersion |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ObjectBuilder.BuilderVersion[] |
values()
Returns an array that contains the values for this enum.
|
public static final ObjectBuilder.BuilderVersion ORIGINAL
public static final ObjectBuilder.BuilderVersion ONE
public static final ObjectBuilder.BuilderVersion TWO
public static final ObjectBuilder.BuilderVersion THREE
public static final int _ORIGINAL
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static ObjectBuilder.BuilderVersion valueOf(int value)
public static ObjectBuilder.BuilderVersion valueOf(String name)
public static ObjectBuilder.BuilderVersion[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.