public static class ComponentAssembly.OpenComponentStatus extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COULD_NOT_OPEN
The component could not be opened
|
static int |
_DELETED_BY_OPEN
The component was deleted on load as a result of the open
|
static int |
_SUCCESSFULLY_OPENED
The component was opened as expected
|
static ComponentAssembly.OpenComponentStatus |
COULD_NOT_OPEN
The component could not be opened
|
static ComponentAssembly.OpenComponentStatus |
DELETED_BY_OPEN
The component was deleted on load as a result of the open
|
static ComponentAssembly.OpenComponentStatus |
SUCCESSFULLY_OPENED
The component was opened as expected
|
Modifier and Type | Method and Description |
---|---|
static ComponentAssembly.OpenComponentStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComponentAssembly.OpenComponentStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComponentAssembly.OpenComponentStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final ComponentAssembly.OpenComponentStatus SUCCESSFULLY_OPENED
public static final ComponentAssembly.OpenComponentStatus DELETED_BY_OPEN
public static final ComponentAssembly.OpenComponentStatus COULD_NOT_OPEN
public static final int _SUCCESSFULLY_OPENED
public static final int _DELETED_BY_OPEN
public static final int _COULD_NOT_OPEN
public static ComponentAssembly.OpenComponentStatus valueOf(int value)
public static ComponentAssembly.OpenComponentStatus valueOf(String name)
public static ComponentAssembly.OpenComponentStatus[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.