public static class AssembliesGeneralPropertiesBuilder.QuantityOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AS_REQUIRED
Sets the as-required quantity on this component.
|
static int |
_NUMBER
Use either the integer or real value to set the quantity
|
static AssembliesGeneralPropertiesBuilder.QuantityOptions |
AS_REQUIRED
Sets the as-required quantity on this component.
|
static AssembliesGeneralPropertiesBuilder.QuantityOptions |
NUMBER
Use either the integer or real value to set the quantity
|
Modifier and Type | Method and Description |
---|---|
static AssembliesGeneralPropertiesBuilder.QuantityOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssembliesGeneralPropertiesBuilder.QuantityOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssembliesGeneralPropertiesBuilder.QuantityOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final AssembliesGeneralPropertiesBuilder.QuantityOptions NUMBER
public static final AssembliesGeneralPropertiesBuilder.QuantityOptions AS_REQUIRED
public static final int _NUMBER
public static final int _AS_REQUIRED
public static AssembliesGeneralPropertiesBuilder.QuantityOptions valueOf(int value)
public static AssembliesGeneralPropertiesBuilder.QuantityOptions valueOf(String name)
public static AssembliesGeneralPropertiesBuilder.QuantityOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.