public static class SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NO
have no free state
|
static int |
_YES
have free state
|
static SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions |
NO
have no free state
|
static SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions |
YES
have free state
|
Modifier and Type | Method and Description |
---|---|
static SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions YES
public static final SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions NO
public static final int _YES
public static final int _NO
public static SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions valueOf(int value)
public static SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions valueOf(String name)
public static SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.