public static class EditSymbolDisplayBuilder.WidthTypes extends Enum
EditSymbolDisplayBuilder.width()
and
EditSymbolDisplayBuilder.setWidth(nxopen.annotations.EditSymbolDisplayBuilder.WidthTypes)
will set this width type at builder side and
will be used to apply the same on the selected contents after commitModifier and Type | Method and Description |
---|---|
static EditSymbolDisplayBuilder.WidthTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EditSymbolDisplayBuilder.WidthTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EditSymbolDisplayBuilder.WidthTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final EditSymbolDisplayBuilder.WidthTypes THIN
public static final EditSymbolDisplayBuilder.WidthTypes NORMAL
public static final EditSymbolDisplayBuilder.WidthTypes THICK
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_ONE
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_TWO
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_THREE
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_FOUR
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_FIVE
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_SIX
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_SEVEN
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_EIGHT
public static final EditSymbolDisplayBuilder.WidthTypes THICKNESS_NINE
public static final int _THIN
public static final int _NORMAL
public static final int _THICK
public static final int _THICKNESS_ONE
public static final int _THICKNESS_TWO
public static final int _THICKNESS_THREE
public static final int _THICKNESS_FOUR
public static final int _THICKNESS_FIVE
public static final int _THICKNESS_SIX
public static final int _THICKNESS_SEVEN
public static final int _THICKNESS_EIGHT
public static final int _THICKNESS_NINE
public static EditSymbolDisplayBuilder.WidthTypes valueOf(int value)
public static EditSymbolDisplayBuilder.WidthTypes valueOf(String name)
public static EditSymbolDisplayBuilder.WidthTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.