public class Constants extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAX_LEADER_INTERMEDIATE_POINTS
The maximum number of intermediate points that a leader can have
|
static int |
_MAX_LEADERS
The maximum number of leaders that an annotation can have
|
static Constants |
MAX_LEADER_INTERMEDIATE_POINTS
The maximum number of intermediate points that a leader can have
|
static Constants |
MAX_LEADERS
The maximum number of leaders that an annotation can have
|
Modifier and Type | Method and Description |
---|---|
static Constants |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Constants |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Constants[] |
values()
Returns an array that contains the values for this enum.
|
public static final Constants MAX_LEADERS
public static final Constants MAX_LEADER_INTERMEDIATE_POINTS
public static final int _MAX_LEADERS
public static final int _MAX_LEADER_INTERMEDIATE_POINTS
public static Constants valueOf(int value)
public static Constants valueOf(String name)
public static Constants[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.