public interface BaseCenterMarkBuilder extends CenterlineBuilder
Property | Value |
---|---|
Settings.Angle | 0 |
Settings.AssociativeAngle.Angle.Value | 0 |
Settings.AssociativeAngle.Associative | 0 |
Settings.AssociativeAngle.EvaluationPlane | DrawingSheet |
Settings.Extension | 6.35 (millimeters part), 0.25 (inches part) |
Settings.Gap | 1.5875 (millimeters part), 0.0625 (inches part) |
Settings.IndividualDistance | 0 |
Settings.InheritAngle | 0 |
Settings.ShowCenterPoint | 0 |
Settings.Size | 3.175 (millimeters part), 0.125 (inches part) |
Settings.Width | Thin |
Modifier and Type | Method and Description |
---|---|
SelectNXObjectList |
locations()
Returns the location object
License requirements: None. |
boolean |
multipleCenterMarks()
Returns the multiple center marks option, applicable only for creation
License requirements: None. |
void |
removeLocation(int index)
Removes location object for a given index from the Select Object List.
|
void |
setMultipleCenterMarks(boolean multipleCenterlines)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
CenterMarkSettingsBuilder |
settings()
Returns the center mark settings builder
License requirements: None. |
addEndExtensions, addExtension, getAllExtensions, getAllIndividualExtensions, getEndExtensions, removeEndExtensions, removeExtension, resetAllExtensions, setAllIndividualExtensions, setEndExtensions, setIndividualExtensions
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectNXObjectList locations() throws NXException, RemoteException
NXException
RemoteException
CenterMarkSettingsBuilder settings() throws NXException, RemoteException
NXException
RemoteException
boolean multipleCenterMarks() throws NXException, RemoteException
NXException
RemoteException
void setMultipleCenterMarks(boolean multipleCenterlines) throws NXException, RemoteException
multipleCenterlines
- NXException
RemoteException
void removeLocation(int index) throws NXException, RemoteException
index
- Index of the object in the select object listNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.