public class AssociativityLineOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANGLE
At angle
|
static int |
_BASE_LINE
Base line
|
static int |
_CENTERLINE
Centerline -
Linear Bolt circle Circular |
static int |
_EXISTING_LINE
Existing line
|
static int |
_EXTENSION_LINE
Extension line
|
static int |
_HORIZONTAL_LEFT
Horizontal left
|
static int |
_HORIZONTAL_RIGHT
Horizontal right
|
static int |
_LAST
Last enum value.
|
static int |
_NONE
No line
|
static int |
_POINT_VECTOR
Vector from two points
|
static int |
_VERTICAL_DOWN
Vertical down
|
static int |
_VERTICAL_UP
Vertical up
|
static AssociativityLineOption |
ANGLE
At angle
|
static AssociativityLineOption |
BASE_LINE
Base line
|
static AssociativityLineOption |
CENTERLINE
Centerline -
Linear Bolt circle Circular |
static AssociativityLineOption |
EXISTING_LINE
Existing line
|
static AssociativityLineOption |
EXTENSION_LINE
Extension line
|
static AssociativityLineOption |
HORIZONTAL_LEFT
Horizontal left
|
static AssociativityLineOption |
HORIZONTAL_RIGHT
Horizontal right
|
static AssociativityLineOption |
LAST
Last enum value.
|
static AssociativityLineOption |
NONE
No line
|
static AssociativityLineOption |
POINT_VECTOR
Vector from two points
|
static AssociativityLineOption |
VERTICAL_DOWN
Vertical down
|
static AssociativityLineOption |
VERTICAL_UP
Vertical up
|
Modifier and Type | Method and Description |
---|---|
static AssociativityLineOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativityLineOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativityLineOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final AssociativityLineOption NONE
public static final AssociativityLineOption EXISTING_LINE
public static final AssociativityLineOption POINT_VECTOR
public static final AssociativityLineOption EXTENSION_LINE
public static final AssociativityLineOption CENTERLINE
public static final AssociativityLineOption ANGLE
public static final AssociativityLineOption HORIZONTAL_RIGHT
public static final AssociativityLineOption VERTICAL_UP
public static final AssociativityLineOption HORIZONTAL_LEFT
public static final AssociativityLineOption VERTICAL_DOWN
public static final AssociativityLineOption BASE_LINE
public static final AssociativityLineOption LAST
public static final int _NONE
public static final int _EXISTING_LINE
public static final int _POINT_VECTOR
public static final int _EXTENSION_LINE
public static final int _CENTERLINE
public static final int _ANGLE
public static final int _HORIZONTAL_RIGHT
public static final int _VERTICAL_UP
public static final int _HORIZONTAL_LEFT
public static final int _VERTICAL_DOWN
public static final int _BASE_LINE
public static final int _LAST
public static AssociativityLineOption valueOf(int value)
public static AssociativityLineOption valueOf(String name)
public static AssociativityLineOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.