public static class SymbolAnnotationBuilder.Orientation extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL |
static int |
_VERTICAL |
static SymbolAnnotationBuilder.Orientation |
HORIZONTAL |
static SymbolAnnotationBuilder.Orientation |
VERTICAL |
Modifier and Type | Method and Description |
---|---|
static SymbolAnnotationBuilder.Orientation |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SymbolAnnotationBuilder.Orientation |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SymbolAnnotationBuilder.Orientation[] |
values()
Returns an array that contains the values for this enum.
|
public static final SymbolAnnotationBuilder.Orientation HORIZONTAL
public static final SymbolAnnotationBuilder.Orientation VERTICAL
public static final int _HORIZONTAL
public static final int _VERTICAL
public static SymbolAnnotationBuilder.Orientation valueOf(int value)
public static SymbolAnnotationBuilder.Orientation valueOf(String name)
public static SymbolAnnotationBuilder.Orientation[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.