public class ImportType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADD_CHILDREN |
static int |
_ADD_FUNCTION |
static int |
_ADD_TYPE |
static ImportType |
ADD_CHILDREN |
static ImportType |
ADD_FUNCTION |
static ImportType |
ADD_TYPE |
Modifier and Type | Method and Description |
---|---|
static ImportType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ImportType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ImportType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ImportType ADD_TYPE
public static final ImportType ADD_FUNCTION
public static final ImportType ADD_CHILDREN
public static final int _ADD_TYPE
public static final int _ADD_FUNCTION
public static final int _ADD_CHILDREN
public static ImportType valueOf(int value)
public static ImportType valueOf(String name)
public static ImportType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.