public static class ElectricalAnnotationSettingsBuilder.AnnotationAttrType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COLOR |
static int |
_CROSS_SECTION |
static int |
_SOURCE_TARGET |
static int |
_WIRE_TYPE |
static ElectricalAnnotationSettingsBuilder.AnnotationAttrType |
COLOR |
static ElectricalAnnotationSettingsBuilder.AnnotationAttrType |
CROSS_SECTION |
static ElectricalAnnotationSettingsBuilder.AnnotationAttrType |
SOURCE_TARGET |
static ElectricalAnnotationSettingsBuilder.AnnotationAttrType |
WIRE_TYPE |
Modifier and Type | Method and Description |
---|---|
static ElectricalAnnotationSettingsBuilder.AnnotationAttrType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElectricalAnnotationSettingsBuilder.AnnotationAttrType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElectricalAnnotationSettingsBuilder.AnnotationAttrType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ElectricalAnnotationSettingsBuilder.AnnotationAttrType SOURCE_TARGET
public static final ElectricalAnnotationSettingsBuilder.AnnotationAttrType CROSS_SECTION
public static final ElectricalAnnotationSettingsBuilder.AnnotationAttrType COLOR
public static final ElectricalAnnotationSettingsBuilder.AnnotationAttrType WIRE_TYPE
public static final int _SOURCE_TARGET
public static final int _CROSS_SECTION
public static final int _COLOR
public static final int _WIRE_TYPE
public static ElectricalAnnotationSettingsBuilder.AnnotationAttrType valueOf(int value)
public static ElectricalAnnotationSettingsBuilder.AnnotationAttrType valueOf(String name)
public static ElectricalAnnotationSettingsBuilder.AnnotationAttrType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.