public static class EditClauseBuilder.Operator extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AS |
static int |
_OF_TYPE |
static int |
_UNDER |
static EditClauseBuilder.Operator |
AS |
static EditClauseBuilder.Operator |
OF_TYPE |
static EditClauseBuilder.Operator |
UNDER |
Modifier and Type | Method and Description |
---|---|
static EditClauseBuilder.Operator |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EditClauseBuilder.Operator |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EditClauseBuilder.Operator[] |
values()
Returns an array that contains the values for this enum.
|
public static final EditClauseBuilder.Operator AS
public static final EditClauseBuilder.Operator UNDER
public static final EditClauseBuilder.Operator OF_TYPE
public static final int _AS
public static final int _UNDER
public static final int _OF_TYPE
public static EditClauseBuilder.Operator valueOf(int value)
public static EditClauseBuilder.Operator valueOf(String name)
public static EditClauseBuilder.Operator[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.