public static class AspectPrefixBuilder.DelimiterType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ASPECT_PREFIX
Aspect Prefix is used as the delimiter
|
static int |
_DOT
A dot (.) is used as the delimiter
|
static int |
_NO_DELIMITER
No delimiter will be used
|
static AspectPrefixBuilder.DelimiterType |
ASPECT_PREFIX
Aspect Prefix is used as the delimiter
|
static AspectPrefixBuilder.DelimiterType |
DOT
A dot (.) is used as the delimiter
|
static AspectPrefixBuilder.DelimiterType |
NO_DELIMITER
No delimiter will be used
|
Modifier and Type | Method and Description |
---|---|
static AspectPrefixBuilder.DelimiterType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AspectPrefixBuilder.DelimiterType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AspectPrefixBuilder.DelimiterType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AspectPrefixBuilder.DelimiterType DOT
public static final AspectPrefixBuilder.DelimiterType ASPECT_PREFIX
public static final AspectPrefixBuilder.DelimiterType NO_DELIMITER
public static final int _DOT
public static final int _ASPECT_PREFIX
public static final int _NO_DELIMITER
public static AspectPrefixBuilder.DelimiterType valueOf(int value)
public static AspectPrefixBuilder.DelimiterType valueOf(String name)
public static AspectPrefixBuilder.DelimiterType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.