public class AddressObjectIotype extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EMPTY |
static int |
_INPUT |
static int |
_OUTPUT |
static AddressObjectIotype |
EMPTY |
static AddressObjectIotype |
INPUT |
static AddressObjectIotype |
OUTPUT |
Modifier and Type | Method and Description |
---|---|
static AddressObjectIotype |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddressObjectIotype |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddressObjectIotype[] |
values()
Returns an array that contains the values for this enum.
|
public static final AddressObjectIotype EMPTY
public static final AddressObjectIotype INPUT
public static final AddressObjectIotype OUTPUT
public static final int _EMPTY
public static final int _INPUT
public static final int _OUTPUT
public static AddressObjectIotype valueOf(int value)
public static AddressObjectIotype valueOf(String name)
public static AddressObjectIotype[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.