public interface VirtuallabImporter extends Builder
VirtuallabImporter
to be used when importing the Virtuallab Data
This class is created using DexManager
.
NULL object will be returned from Commit() DexManager.createVirtuallabImporter()
Property | Value |
---|---|
UseFileDirectory | 1 |
Modifier and Type | Method and Description |
---|---|
String |
outputDirectory()
Returns the output directory - where the sim file will be created
License requirements: None. |
void |
saveSettings(String filename)
Save the settings - this will save the settings to a file specified
License requirements: None. |
void |
setOutputDirectory(String outputDirectory)
License requirements: None. |
void |
setSettingsFile(String filename)
License requirements: None. |
String |
settingsFile()
Returns the settings file - definition file for default options
License requirements: None. |
void |
setUseFileDirectory(boolean useFileDirectory)
License requirements: None. |
boolean |
useFileDirectory()
Returns the use file directory - if set to true then sim files will be created in the same directory as the input file
License requirements: None. |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
void saveSettings(String filename) throws NXException, RemoteException
filename
- NXException
RemoteException
String settingsFile() throws NXException, RemoteException
NXException
RemoteException
void setSettingsFile(String filename) throws NXException, RemoteException
filename
- NXException
RemoteException
boolean useFileDirectory() throws NXException, RemoteException
NXException
RemoteException
void setUseFileDirectory(boolean useFileDirectory) throws NXException, RemoteException
useFileDirectory
- NXException
RemoteException
String outputDirectory() throws NXException, RemoteException
NXException
RemoteException
void setOutputDirectory(String outputDirectory) throws NXException, RemoteException
outputDirectory
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.