public static class PreviewPropertiesBuilder.PartCreationOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ON_DEMAND
Interactive only option that allows the part preview to be created by selecting the Create Now button
|
static int |
_ON_SAVE
Part preview will be created when the part is saved
|
static PreviewPropertiesBuilder.PartCreationOptions |
ON_DEMAND
Interactive only option that allows the part preview to be created by selecting the Create Now button
|
static PreviewPropertiesBuilder.PartCreationOptions |
ON_SAVE
Part preview will be created when the part is saved
|
Modifier and Type | Method and Description |
---|---|
static PreviewPropertiesBuilder.PartCreationOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PreviewPropertiesBuilder.PartCreationOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PreviewPropertiesBuilder.PartCreationOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final PreviewPropertiesBuilder.PartCreationOptions ON_SAVE
public static final PreviewPropertiesBuilder.PartCreationOptions ON_DEMAND
public static final int _ON_SAVE
public static final int _ON_DEMAND
public static PreviewPropertiesBuilder.PartCreationOptions valueOf(int value)
public static PreviewPropertiesBuilder.PartCreationOptions valueOf(String name)
public static PreviewPropertiesBuilder.PartCreationOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.