public static class PointCollection.AlongCurveOption extends Enum
PointCollection.createPoint(nxopen.Point3d)
method is either an absolute distance or a relative percentage.Modifier and Type | Field and Description |
---|---|
static int |
_DISTANCE
Scalar is an absolute distance.
|
static int |
_PERCENT
Scalar is a relative percentage.
|
static PointCollection.AlongCurveOption |
DISTANCE
Scalar is an absolute distance.
|
static PointCollection.AlongCurveOption |
PERCENT
Scalar is a relative percentage.
|
Modifier and Type | Method and Description |
---|---|
static PointCollection.AlongCurveOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointCollection.AlongCurveOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointCollection.AlongCurveOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final PointCollection.AlongCurveOption DISTANCE
public static final PointCollection.AlongCurveOption PERCENT
public static final int _DISTANCE
public static final int _PERCENT
public static PointCollection.AlongCurveOption valueOf(int value)
public static PointCollection.AlongCurveOption valueOf(String name)
public static PointCollection.AlongCurveOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.