public class PartDisplayPartWorkPartOption extends Enum
PartCollection.setActiveDisplay(nxopen.BasePart, nxopen.DisplayPartOption, nxopen.PartDisplayPartWorkPartOption)
Modifier and Type | Field and Description |
---|---|
static int |
_SAME_AS_DISPLAY
New work part will be set to the new display part
|
static int |
_USE_LAST
If possible use the work part that was used when this part was last the display part
|
static PartDisplayPartWorkPartOption |
SAME_AS_DISPLAY
New work part will be set to the new display part
|
static PartDisplayPartWorkPartOption |
USE_LAST
If possible use the work part that was used when this part was last the display part
|
Modifier and Type | Method and Description |
---|---|
static PartDisplayPartWorkPartOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartDisplayPartWorkPartOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartDisplayPartWorkPartOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartDisplayPartWorkPartOption SAME_AS_DISPLAY
public static final PartDisplayPartWorkPartOption USE_LAST
public static final int _SAME_AS_DISPLAY
public static final int _USE_LAST
public static PartDisplayPartWorkPartOption valueOf(int value)
public static PartDisplayPartWorkPartOption valueOf(String name)
public static PartDisplayPartWorkPartOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.