public interface FloodFillFacetsRule extends FacetSelectionRule
FloodFillFacetsRule
that collects flood filled facets.
This rule expands to add all neighboring facets of seed (and the neighbor-neighbors)
until the region reaches a closed ring of already collected facets in collector.
If already collected facets in collector do not form a closed ring, then the rule expands
to all the facets of owning face of the seed.
Modifier and Type | Interface and Description |
---|---|
static class |
FloodFillFacetsRule.Data
This class holds the data returned from
getData() |
Modifier and Type | Method and Description |
---|---|
FloodFillFacetsRule.Data |
getData()
Gets the data for the flood fill facets rule:
FloodFillFacetsRule
License requirements: gateway ("UG GATEWAY") Created in NX12.0.0 |
_value, dispose, printTestData, printTestData
FloodFillFacetsRule.Data getData() throws NXException, RemoteException
FloodFillFacetsRule
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.