public class DisplayPartOption extends Enum
PartCollection.setActiveDisplay(nxopen.BasePart, nxopen.DisplayPartOption, nxopen.PartDisplayPartWorkPartOption)
Modifier and Type | Field and Description |
---|---|
static int |
_ALLOW_ADDITIONAL
If possible display the new part as an additional display part
|
static int |
_REPLACE_EXISTING
Replace the existing active display part with the new one
|
static DisplayPartOption |
ALLOW_ADDITIONAL
If possible display the new part as an additional display part
|
static DisplayPartOption |
REPLACE_EXISTING
Replace the existing active display part with the new one
|
Modifier and Type | Method and Description |
---|---|
static DisplayPartOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayPartOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayPartOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final DisplayPartOption REPLACE_EXISTING
public static final DisplayPartOption ALLOW_ADDITIONAL
public static final int _REPLACE_EXISTING
public static final int _ALLOW_ADDITIONAL
public static DisplayPartOption valueOf(int value)
public static DisplayPartOption valueOf(String name)
public static DisplayPartOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.