public static class CGMBuilder.SizeOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DIMENSION
Dimension, uses the units along with X and Y dimensions to determine CGM size
|
static int |
_FULL_SCALE
Full Scale
|
static int |
_SCALE_FACTOR
Scale Factor, scales the CGM based on user defined scale field
|
static CGMBuilder.SizeOption |
DIMENSION
Dimension, uses the units along with X and Y dimensions to determine CGM size
|
static CGMBuilder.SizeOption |
FULL_SCALE
Full Scale
|
static CGMBuilder.SizeOption |
SCALE_FACTOR
Scale Factor, scales the CGM based on user defined scale field
|
Modifier and Type | Method and Description |
---|---|
static CGMBuilder.SizeOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CGMBuilder.SizeOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CGMBuilder.SizeOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final CGMBuilder.SizeOption FULL_SCALE
public static final CGMBuilder.SizeOption SCALE_FACTOR
public static final CGMBuilder.SizeOption DIMENSION
public static final int _FULL_SCALE
public static final int _SCALE_FACTOR
public static final int _DIMENSION
public static CGMBuilder.SizeOption valueOf(int value)
public static CGMBuilder.SizeOption valueOf(String name)
public static CGMBuilder.SizeOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.