public interface AttributePropertiesBuilder extends AttributePropertiesBaseBuilder
AttributePropertiesBuilder
. Input to this class can be PSM facet objects.
AttributeManager.createAttributePropertiesBuilder(nxopen.BasePart, nxopen.NXObject[], nxopen.AttributePropertiesBuilder.OperationType)
Property | Value |
---|---|
BooleanValue | False |
DataType | String |
IntegerValue | 0 |
NumberValue | 0 |
ObjectPicker (deprecated) | Object |
Modifier and Type | Interface and Description |
---|---|
static class |
AttributePropertiesBuilder.OperationType
It is used to determine the behaviors of attributes that has been mapped from TC,
such as Hidden, Required, CopyFromOriginal, etc.
|
AttributePropertiesBaseBuilder.BooleanValueOptions, AttributePropertiesBaseBuilder.DataTypeOptions, AttributePropertiesBaseBuilder.ObjectOptions
applyUnits, arrayIndex, booleanValue, category, createAttribute, dataType, dateValue, delete, deleteArray, expression, integerValue, isArray, isReferenceType, lockOnSave, numberValue, objectPicker, selectedObjects, setArray, setArrayIndex, setAttributeObjects, setBooleanValue, setCategory, setDataType, setExpression, setIntegerValue, setLockOnSave, setNumberValue, setObjectPicker, setReferenceType, setStringValue, setTitle, setUnits, setValueAlias, stringValue, title, units, valueAlias
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.