WeldDebugSession Class¶
-
class
NXOpen.
WeldDebugSession
¶ Bases:
object
Represents a class that is used for NX WELD Autotest.
This class should not be made available to customers To obtain an instance of this class, refer to
NXOpen.DebugSession
New in version NX11.0.2.
Methods¶
Method | Description |
---|---|
CreateWeldValidator | Create a weld validation object. |
PopulateValidators | Create the validators for each weld feature found. |
Method Detail¶
CreateWeldValidator¶
-
WeldDebugSession.
CreateWeldValidator
¶ Create a weld validation object.
Doubles will have the following tolerances assigned: if 0.0, then always uses absolute tolerance. If not equal to 0.0, then use relative tolerance unless the isAbsoluteTolerance is true.
Signature
CreateWeldValidator(displayPart, featMask, absoluteTolerance, relativeTolerance, isAbsoluteTolerance)
Parameters: - displayPart (
NXOpen.BasePart
) – part being validated - featMask (int) –
- absoluteTolerance (float) –
- relativeTolerance (float) –
- isAbsoluteTolerance (bool) –
Returns: created validator
Return type: New in version NX11.0.2.
License requirements: None.
- displayPart (
PopulateValidators¶
-
WeldDebugSession.
PopulateValidators
¶ Create the validators for each weld feature found.
Signature
PopulateValidators(mainValidator)
Parameters: mainValidator ( NXOpen.WeldBaseValidator
) – main weld validatorReturns: created validators Return type: list of NXOpen.WeldBaseValidator
New in version NX11.0.2.
License requirements: None.