WeldSpacingCalcMethod Enumeration¶
-
class
NXOpen.Weld.
WeldSpacingCalcMethod
¶ Bases:
object
Settings spacing method type Enum Members
Enum Member Enum Member Description Arclength spaces based on arc length ParallelXPlane spaces based on parallel x planes ParallelYPlane spaces based on parallel y planes ParallelZPlane spaces based on parallel z planes MiddleOfCurve spaces based on middle of curve NormalToBody spaces based on normal to body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-