WeldPrepareEdges Enumeration¶
-
class
NXOpen.Weld.
WeldPrepareEdges
¶ Bases:
object
Settings for prepare edges Enum Members
Enum Member Enum Member Description NotSet Output edges will not be prepared EntireEdge Output edges will be prepared for entire edge length WeldLimits Output edges will be prepared for the weld length only Complex Same as entire edge, but use if a portion of target body is below the desired weld -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-