WeldPointMethod Enumeration¶
-
class
NXOpen.Weld.
WeldPointMethod
¶ Bases:
object
Settings for method Enum Members
Enum Member Enum Member Description Multiple use guide curve(s) or edge(s) to generate spot weld points Single use point constructor to generate spot weld points Mirror mirror existing points Translate translate existing points FromPoints create fix/single/none points using existing points -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-