WeldObjectBuilderCommandName Enumeration¶
NXOpen.Weld.WeldObjectBuilder.CommandName is an alias for NXOpen.Weld.WeldObjectBuilderCommandName
-
class
NXOpen.Weld.
WeldObjectBuilderCommandName
¶ Bases:
object
Commands that a callback will be invoked after dialog completion.
Enum Members
Enum Member Enum Member Description NotSet No command. Used to initialize value. Groove Groove Weld command Fillet Fillet Weld command UserDefined User Defined Weld command WeldPoint Weld Point command Bead Bead command Fill Fill command ImportCsv Import CSV command EasySpot Easy Spot command DatumLocator Datum Locator command MeasurementLocator Measurement Locator command EasyMeasurementPattern Easy Measurement Pattern command PlugSlot Plug Slot command Joint Welding Joint command DatumSurface Datum Surface command DatumPin Datum Pin command SurfaceWeld Surface Weld command Compound Compound Weld command WeldAttribute Edit Weld Attribute JointDefinition Edit Joint Definition Parameters Jointmark Joint Mark command WeldPointWizard Weld Point Wizard command Transform Weld Transform command -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-