WeldLabelBuilderOrientationPlaneType Enumeration

NXOpen.Weld.WeldLabelBuilder.OrientationPlaneType is an alias for NXOpen.Weld.WeldLabelBuilderOrientationPlaneType

class NXOpen.Weld.WeldLabelBuilderOrientationPlaneType

Bases: object

This represents the Orientation Plane Type.

Enum Members

Enum Member Enum Member Description
XYPlane
XZPlane
YZPlane
ModelView
LastUserDefined
UserDefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.