WeldJointBuilderCoordinateSystem Enumeration¶
NXOpen.Weld.WeldJointBuilder.CoordinateSystem is an alias for NXOpen.Weld.WeldJointBuilderCoordinateSystem
-
class
NXOpen.Weld.
WeldJointBuilderCoordinateSystem
¶ Bases:
object
Coordinate system specification.
Enum Members
Enum Member Enum Member Description Absolute Desired points and vectors should be in absolute coordinates. Ship Desired points and vectors should be in ship coordinate system. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-