WeldGrooveExtension Enumeration¶
-
class
NXOpen.Weld.
WeldGrooveExtension
¶ Bases:
object
Groove Extension Type Enum Members
Enum Member Enum Member Description Tangent Extend selected edges to form an intersection. Project Project selected edges to opposite face set. ReverseProject Project selected edges to oppsoite face set using normals from selected edges. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-