WeldFillBuilderWidthAlongType Enumeration¶
NXOpen.Weld.WeldFillBuilder.WidthAlongType is an alias for NXOpen.Weld.WeldFillBuilderWidthAlongType
-
class
NXOpen.Weld.
WeldFillBuilderWidthAlongType
¶ Bases:
object
Defines the direction the fill strip’s length is aligned
Enum Members
Enum Member Enum Member Description Xc The length is aligned along the current WCS X direction. Yc The length is aligned along the current WCS Y direction. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-