WeldFeatureSetType Enumeration¶
-
class
NXOpen.Weld.
WeldFeatureSetType
¶ Bases:
object
the feature set types Enum Members
Enum Member Enum Member Description FilletWeld Fillet Weld GrooveWeld Groove Weld ResistanceSpot Resistance Spot ArcSpot Arc Spot Clinch Clinch Dollop Dollop WeldNut Weld Nut WeldStud Weld Stud Custom1Point Custom1 Point Custom2Point Custom2 Point Custom3Point Custom3 Point Custom4Point Custom4 Point Custom5Point Custom5 Point BiwDatumSurface Datum Surface BiwDatumPin Datum Pin BiwDatumCustomer1 Datum Customer1 BiwDatumCustomer2 Datum Customer2 BiwDatumCustomer3 Datum Customer3 BiwMeasurementSurface Measurement Surface BiwMeasurementHole Measurement Hole BiwMeasurementSlot Measurement Slot BiwMeasurementStud Measurement Stud BiwMeasurementTrim Measurement Trim BiwMeasurementHem Measurement Hem BiwMeasurementCustomer1 Measurement Customer1 BiwMeasurementCustomer2 Measurement Customer2 BiwMeasurementCustomer3 Measurement Customer3 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-