WeldBeadBuilderTypes Enumeration¶
NXOpen.Weld.WeldBeadBuilder.Types is an alias for NXOpen.Weld.WeldBeadBuilderTypes
-
class
NXOpen.Weld.
WeldBeadBuilderTypes
¶ Bases:
object
Settings to indicate the sweep shape of the bead.
Enum Members
Enum Member Enum Member Description Ellipse ellipse shape Tube tube shape Sketch sketch shape Triangle triangle shape Rectangle rectangle shape -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-