WeldBeadBuilderFaceInferMethodType Enumeration¶
NXOpen.Weld.WeldBeadBuilder.FaceInferMethodType is an alias for NXOpen.Weld.WeldBeadBuilderFaceInferMethodType
-
class
NXOpen.Weld.
WeldBeadBuilderFaceInferMethodType
¶ Bases:
object
Settings to indicate the method for obtaining faces used when creating the guide curve path.
Enum Members
Enum Member Enum Member Description TangentFaces use faces tangent to selected faces to create the bead path curve NotSet only use selected faces to create the bead path curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-