WeldBeadBuilderBeadLocationMethod Enumeration¶
NXOpen.Weld.WeldBeadBuilder.BeadLocationMethod is an alias for NXOpen.Weld.WeldBeadBuilderBeadLocationMethod
-
class
NXOpen.Weld.
WeldBeadBuilderBeadLocationMethod
¶ Bases:
object
Settings to indicate the desired location of the bead.
Enum Members
Enum Member Enum Member Description SecondaryParts on the secondary parts PrimaryParts on the primary parts InSpace in space. No on any parts -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-