WeldAdvisorCustomerDefault Enumeration¶
-
class
NXOpen.Weld.
WeldAdvisorCustomerDefault
¶ Bases:
object
the customer default value types Enum Members
Enum Member Enum Member Description ResistanceSpot Resistance Spot ArcSpot Arc Spot Clinch Clinch Dollop Dollop WeldNut Weld Nut WeldStud Weld Stud Custom1Point Custom1 Point Custom2Point Custom2 Point Custom3Point Custom3 Point Custom4Point Custom4 Point Custom5Point Custom5 Point Datum datum, used for implementing weld advisor parameters Measurement measurement, used for implementing weld advisor parameters Num number of types -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-