WeldAdvisorCheckerType Enumeration¶
-
class
NXOpen.Weld.
WeldAdvisorCheckerType
¶ Bases:
object
the type of checker Enum Members
Enum Member Enum Member Description CoincidentPoint Mimimum Distance MinimumPointDistance minimum point distance MinimumEdgeDistance minimum edge distance StackUpGap stack up gap FacePlanarity face planarity FaceParallelism face parallelism PointFaceDistance point face distance CsysFaceNormalAngle csys face normal angle MetalStackUp metal stack up MetalMinimumPointDatumDistance minimum point datum distance MetalMinimumPointMeasurementDistance minimum point measurement distance SpacingPerPanelCombination spacing per panel combination WeldFlange weld flange Bead sealer bead Number number of checkers -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-