UserDefinedWeldBuilderWeldTypes Enumeration¶
NXOpen.Weld.UserDefinedWeldBuilder.WeldTypes is an alias for NXOpen.Weld.UserDefinedWeldBuilderWeldTypes
-
class
NXOpen.Weld.
UserDefinedWeldBuilderWeldTypes
¶ Bases:
object
Weld types for 4GD classes.
Enum Members
Enum Member Enum Member Description Groove Groove Weld type. Fillet Fillet Weld type. PlugSlot Plug Slot Weld type. Bead Bead Weld type. Fill Fill Weld type. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-