TransformBuilderConnectedPartMethods Enumeration¶
NXOpen.Weld.TransformBuilder.ConnectedPartMethods is an alias for NXOpen.Weld.TransformBuilderConnectedPartMethods
-
class
NXOpen.Weld.
TransformBuilderConnectedPartMethods
¶ Bases:
object
The type to define the method used to find connected parts
Enum Members
Enum Member Enum Member Description TransformBody Use the location of the transform body to help find connected parts ParentFaces Use transformed parent faces to find connected parts -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-