SurfaceWeldBuilderDestinationTypes Enumeration

NXOpen.Weld.SurfaceWeldBuilder.DestinationTypes is an alias for NXOpen.Weld.SurfaceWeldBuilderDestinationTypes

class NXOpen.Weld.SurfaceWeldBuilderDestinationTypes

Bases: object

The option specifying where the surface weld feature should be created.

Enum Members

Enum Member Enum Member Description
WorkPart
NewComponent
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.