PointMarkPointBuilder Class

class NXOpen.Weld.PointMarkPointBuilder

Bases: NXOpen.Weld.JointmarkPointsBuilder

Used to create or edit a point in the list of points for Jointmark

To create a new instance of this class, use NXOpen.Weld.PointMarkBuilder.NewPointsOverride()

New in version NX10.0.0.

Properties

Property Description
Angle Returns the angle through which X and Y axis to rotate
FlipDirection Returns or sets the flip of Z axis.
MappingFeature Returns the selected feature to move to the location specified.
Point Returns or sets the point at which the feature is created
Tag Returns the Tag for this object.

Methods

Method Description
UpdateCsys Update the csys using a new matrix.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

Validate

PointMarkPointBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.