PointMarkBuilderWeldTypes Enumeration¶
NXOpen.Weld.PointMarkBuilder.WeldTypes is an alias for NXOpen.Weld.PointMarkBuilderWeldTypes
-
class
NXOpen.Weld.
PointMarkBuilderWeldTypes
¶ Bases:
object
The weld type to create.
Enum Members
Enum Member Enum Member Description ResistanceSpot Resistance Spot ArcSpot Arc Spot Clinch Clinch Dollop Dollop WeldNut Weld Nut WeldStud Weld Stud Custom1 Custom 1 as defined in customer defaults Custom2 Custom 2 as defined in customer defaults Custom3 Custom 3 as defined in customer defaults Custom4 Custom 4 as defined in customer defaults Custom5 Custom 5 as defined in customer defaults -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-