PlugSlotBuilderArcProcessEnum Enumeration

NXOpen.Weld.PlugSlotBuilder.ArcProcessEnum is an alias for NXOpen.Weld.PlugSlotBuilderArcProcessEnum

class NXOpen.Weld.PlugSlotBuilderArcProcessEnum

Bases: object

arc process for the weld feature

Enum Members

Enum Member Enum Member Description
Gmaw
Gtaw
Gtac
Smaw
Paw
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.