OutputType Enumeration¶
-
class
NXOpen.Weld.
OutputType
¶ Bases:
object
Settings for output type
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description Associative output data will be associated to inputs. If inputs change the outputs will change also Fixed output data will not change if inputs change -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-