JointmarkGuideBuilderSpaceOption Enumeration¶
NXOpen.Weld.JointmarkGuideBuilder.SpaceOption is an alias for NXOpen.Weld.JointmarkGuideBuilderSpaceOption
-
class
NXOpen.Weld.
JointmarkGuideBuilderSpaceOption
¶ Bases:
object
Spacing Option
Enum Members
Enum Member Enum Member Description Distance Space points by a fixed distance. Spacing at last point may not be uniform. Number Uniformly space a number of points. MinimumDistance Uniformly space points using a minimum distance value. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-