JointmarkBuilderProjectionDirectionOptions Enumeration¶
NXOpen.Weld.JointmarkBuilder.ProjectionDirectionOptions is an alias for NXOpen.Weld.JointmarkBuilderProjectionDirectionOptions
-
class
NXOpen.Weld.
JointmarkBuilderProjectionDirectionOptions
¶ Bases:
object
The projection direction used to project points onto the reference sheet
Enum Members
Enum Member Enum Member Description NotSet AlongFaceNormal PricipalAxis X Y Z -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-