JointmarkBuilderOrientationMethodTypes Enumeration¶
NXOpen.Weld.JointmarkBuilder.OrientationMethodTypes is an alias for NXOpen.Weld.JointmarkBuilderOrientationMethodTypes
-
class
NXOpen.Weld.
JointmarkBuilderOrientationMethodTypes
¶ Bases:
object
The type of orientation method for defining the default coordinate system.
Enum Members
Enum Member Enum Member Description SurfaceNormal Surface Normals. CoordinateSystem Use fixed csys instead of surface normals. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-