JointmarkBuilderMethod Enumeration¶
NXOpen.Weld.JointmarkBuilder.Method is an alias for NXOpen.Weld.JointmarkBuilderMethod
-
class
NXOpen.Weld.
JointmarkBuilderMethod
¶ Bases:
object
The type of construction method for creating Jointmark
Enum Members
Enum Member Enum Member Description GuideCurve Guide Curve Mirror Mirror Points Points Translate Translate ExistingPoints Existing Points. Only allowed for NXOpen.Weld.PointMark
class.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-