JointmarkBuilderConnectedPanelTypes Enumeration

NXOpen.Weld.JointmarkBuilder.ConnectedPanelTypes is an alias for NXOpen.Weld.JointmarkBuilderConnectedPanelTypes

class NXOpen.Weld.JointmarkBuilderConnectedPanelTypes

Bases: object

The type of sheets to create

Enum Members

Enum Member Enum Member Description
Two
Three
Four
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.