InformationBuilderAttributeOriginType Enumeration

NXOpen.Weld.InformationBuilder.AttributeOriginType is an alias for NXOpen.Weld.InformationBuilderAttributeOriginType

class NXOpen.Weld.InformationBuilderAttributeOriginType

Bases: object

the Object Type enum

Enum Members

Enum Member Enum Member Description
Object
Df
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.